AXIS#.MOTOR.TYPE

Description

AXIS#.MOTOR.TYPE sets the motor type and the torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist control algorithm for the motor. The following table provides the motor types:

AXIS#.MOTOR.TYPE Motor and Control Type
0 Rotary surface permanent magnet motor
2 Induction motor with V/Hz open loop control
4 Induction motor with closed loop control
6 Rotary interior permanent magnet motor
8 Rotary brush motor

  • This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.3 or greater.


  • ECCN 3A255 imposes special limitations on operating speed for induction motors. See ECCN 3A225 Limitations for Induction Motors (➜ p. 1).

Each motor type has a set of parameters that must be configured, either through automatically setting them to values in motor memory (when AXIS#.MOTOR.AUTOSET = 1) or through manual user settings. The list of required parameters are reported by AXIS#.SETUPREQLIST, which updates when the motor type changes. When any of the required parameters are not configured, the drive reports Faults and Warning Messages (Drive motor parameters setup incomplete) on the axis.

The following parameters are required for rotary surface permanent magnet motors (AXIS#.MOTOR.TYPE = 0):

The following parameters are required for induction motors with open loop V/f control (AXIS#.MOTOR.TYPE = 2):

The following parameters are required for induction motors with closed loop control (AXIS#.MOTOR.TYPE = 4):

The following parameters are required for rotary interior permanent magnet motors (AXIS#.MOTOR.TYPE = 6):

The following parameters are required for rotary brush motors (AXIS#.MOTOR.TYPE = 8):

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0, 2 ,4, 6, 8

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.TYPE 0x500B 0x4 USINT - - RW False
AXIS2.MOTOR.TYPE 0x510B 0x4 USINT - - RW False